-
How to mitigate interference between multiple LiDAR sensors?
Answer:Interference between multiple LiDAR sensors can be mitigated or even avoided by adding PhaseLock function to the LiDAR or optimizing the LiDAR mounting position.
-
Does RoboSense provide time synchronization board for time synchronization of multiple LiDAR sensors?
Answer:Yes. The time synchronization board is sold as part of RoboSense’s LiDAR perception solutions, please check with your account manager for a quotation.
-
Is the LiDAR laser harmful to human eyes?
Answer:RoboSense LiDAR sensors are certificated with class 1 eye safety according to the IEC/EN 60825-1:2014 standard, which means they are safe under all conditions of normal use.
-
After synchronized with GPS, the UTC time of the point cloud of the LiDAR is 1s or 1s+1 PPS pulse width lagged behind the actual time.
Answer:Currently, this problem only presents in the RS-LiDAR-16, RS-LiDAR-32 and RS-BPearl products. Other products do not have such problem.
(1)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 255 or 0 (Check through RSVIEW-TOOLS-RSLidar info), there will be a lag of 1S+1 PPS pulse width;
(2)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 1, there will be a lag of 1S;
(3)When the time mode of the RS-LiDAR-16, RS-LiDAR-32, and RS-BPearl is 2, the time is synchronized with the current time of GPRMC;
(4)The V3.0 and earlier version of the RS-LiDAR-16, and the V1.7 and earlier version of the RS-Lidar-32 do not support time mode setting;
-
Does the LiDAR currently support Beidou time synchronization?
Answer:Not at the moment. If necessary, please contact RoboSense technical expert to evaluate the feasibility and cost.
-
Will there be a delay after the LiDAR receives a GPS time synchronization signal?
Answer:No.
-
What are the requirements for the power supply?
Answer:(1) The power supply should be stable;
(2) The power supply and current should be able to support stable operation of the LiDAR;
(3) The power supply shall provide sufficient starting current for the LiDAR;
-
When connected to the pluggable space-style bayonet connector, are the LiDAR sensor itself and the interface box waterproof?
Answer:The LiDAR sensor itself is waterproof, but the interface box is not.
-
LiDAR restarts repeatedly or the rotating motor do not start?
Answer:Check the current and voltage output. If you are using modified or extended cable, please also check the voltage drop.
-
Is the pluggable space-style bayonet connector waterproof?
Answer:The connect of RS-LiDAR-16 before v4.0 and that of the RS-LiDAR-32 before v2.0 are not waterproof.